LED Driver: Function, Types, and Application

How To Choose The Correct LED Driver For Your LED Lights
Catalog
I What is an LED Driver?
LED Driver refers to the power adjustment electronic device that drives LED light or LED module components work normally. Due to the conduction characteristics of the LED PN junction, the voltage and current range of the power supply it can adapt to is very narrow, and a slight deviation may not be able to light the LED, or the luminous efficiency will be seriously reduced, or the service life may be shortened or the chip may be burned.
II What Does an Led Driver Do?
The current industrial frequency power supply and common battery power supply are not suitable for directly supplying LEDs. LED drivers are such electronic components that can drive LEDs to work under the best voltage or current state.
Since LED applications are almost universal in various fields of electronics applications, the changes in its luminous intensity, light color, and on-off control are almost unpredictable. So LED drivers become almost one-to-one servo devices, making this device family members become diverse.
The simplest LED driver (if you can call it that way) may be one or several series-parallel resistor-capacitor components that divide the current and divide the voltage in the loop. It is not an independent product at all.
For more general commercial applications requiring stable constant current and constant voltage output, a series of system solutions with precise power adjustment capabilities have been formed. Realizing these solutions usually requires a more complex LED driver circuit design, the core of which is the integrated application of LED driver chips.
By setting up different support circuits on the periphery of the LED driver IC, we can build solutions for different LED applications, ranging from mobile phone display backlight and button lighting drivers to high-power LED street lights and large outdoor LED displays.

Figure 1. LED Driver
The design and supply of common high-power LED driver boards are generally undertaken by professional companies. These companies repackage them into modules and supply them to LED terminal application product manufacturers. The LED driver design of the less general LED terminal application products may need to be designed by yourself.
The LED driver has become an important part of the unique technical content of this LED terminal application product. Because the LED as a packaged product is upstream, its technical performance has been solidified in the LED product, and to create a unique terminal LED application product, for the light source, there are not many places we can work with except for the LED driving function.
Due to the importance of the LED driver in LED application products and the wide user needs, the LED driver IC, which is the heart of the LED driver, has become a key element in the entire technical link. Thus, many manufacturers, or even listed companies, make LED drivers as their main products to supply large quantities of LED driver ICs to downstream industries. There are many leading American LED driver manufacturers, such as National Semiconductor, Maxim, Texas Instruments, ON Semiconductor, Linear Technology, Fairchild Semiconductor, and so on.
The LED drive power supply is a voltage converter that converts the power supply into a specific voltage and current to drive the LED to emit light. Under normal circumstances, the input of the LED drive power includes high-voltage power frequency AC (ie mains), low-voltage DC, high-voltage DC, low-voltage high-frequency AC (such as the output of an electronic transformer), etc. The output of the LED light power supply is mostly a constant current source that can change the voltage with the change of the forward voltage drop of the LED.
III Features
According to the power rules of the power grid and the characteristic requirements of the LED drive power supply, the following points should be considered when we select and design the LED drive power supply:
1. High Reliability
Especially like the driving power of LED street lights, it is inconvenient and expensive to maintain when it's installed at high altitude.
2. High Efficiency
LEDs are energy-saving products, so the efficiency of the drive power supply should be high. For power supply installation, the structure of the LED drive power supply in the lamp is particularly important. Also, because the luminous efficiency of the LED decreases as the temperature of the LED increases, the heat dissipation of the LED is very important. If the efficiency of the power supply is high, its power consumption is small, and the heat generated in the lamp is small, which reduces the temperature rise of the lamp, beneficial to delay the light decay of LED.
3. High Power Factor
The power factor is the requirement of the power grid on the load. Generally, there are no mandatory indicators for electrical appliances below 70 watts. Although a lower power factor of a single electrical appliance with low power has little effect on the power grid, if everyone lights up at night, the similar loads are too concentrated, which will cause serious pollution to the power grid.
It is said that in the near future, there may be certain index requirements for power factors of LED driving power supplies of 30 watts to 40 watts.
4. Driving Methods
There are two common driving methods:
(1) A constant voltage source for multiple constant current sources, and each constant current source individually supplies power to each LED. In this way, the combination is flexible, and the failure of one LED will not affect the work of other LEDs, but the cost will be slightly higher.
(2) Direct constant current power supply, with LED in series or parallel. Its advantage is that the cost is a little lower, but the flexibility is poor, and it must solve the problem of a certain LED failure without affecting the operation of other LEDs.

Figure 2. Constant Voltage LED Driver
These two forms coexist for a period of time. The power supply mode of multi-channel constant current output will be better in terms of cost and performance, which may become the mainstream direction in the future.
5. Surge Protection
The ability of LEDs to resist surges is relatively poor, especially the ability to resist reverse voltage. So, it is important to strengthen protection in this area.
Some LED lights are installed outdoors, such as LED street lights. Due to the onset of the grid load and the induction of lightning strikes, various surges will invade into the grid system, and some surges will cause damage to the LED. Therefore, the LED drive power supply must have the ability to suppress the intrusion of surges and protect the LED from damage.
6. Protection Function
In addition to the common protection function of the LED power supply, it is better to add negative feedback of LED temperature to the constant current output to prevent the LED temperature from being too high.
7. In terms of protection, the lamp is externally mounted, the power supply structure must be waterproof and moisture-proof, and the outer shell must be lightfast.
8. The life of the driving power supply should be matched with the life of the LED.
9. Requirements of safety regulations and electromagnetic compatibility
With the increasing application of LEDs, the performance of LED driving power will be more and more suitable for LED requirements.
IV LED Driver Types
1. According to the Drive Mode
(1) Constant Current Led Driver
1) The output current of the constant current LED drive circuit is constant, but the output DC voltage varies within a certain range with the change of the load resistance. The smaller the load resistance, the lower the output voltage. The larger the load resistance, the higher the output voltage;
2) The load short is allowed to occur in the constant current circuit, but the load can not be open completely.
3) It is ideal for a constant current LED driver circuit to drive LEDs, but it is relatively expensive.
4) Pay attention to the maximum withstand current and voltage values used, which limit the number of LEDs used;
(2) Regulated LED Driver
1) When the various parameters in the voltage regulator circuit are determined, the output voltage is fixed, but the output current changes with the increase or decrease of the load;
2) In the voltage regulator circuit, load opening is allowed, but it is strictly forbidden to short-circuit the load completely.
3) The LED is driven by a voltage-stabilizing LED driving circuit, and each string needs to be added with a suitable resistor to make the brightness of each LED string average;
4) Brightness will be affected by voltage changes from rectification.
2. According to the Circuit Structure
(1) Capacitor Step-down Method
When the capacitor is used to reduce the voltage, due to the effect of charging and discharging, the instantaneous current through the LED is extremely large, and the chip is easily damaged. The method is easily affected by the fluctuation of the grid voltage, and the power supply has low efficiency and low reliability.
(2) Resistor Step-down Method
The resistor step-down is greatly affected by the change of the grid voltage, and it is not easy to make a regulated power supply. The step-down resistor consumes a large part of the energy, so this power supply method has low efficiency, and the system has low reliability.
(3) Conventional Transformer step-down Method
The power supply is small, heavy, and has low power supply efficiency, generally only 45% to 60%, so it generally has low reliability and is rarely used.
(4) Electronic Transformer Step-down Method
The power supply efficiency is low, and the voltage range is not wide, generally 180-240V, with large ripple interference.
(5) RCC Step-down Switching Power Supply
The voltage regulation range is relatively wide, the power supply efficiency is relatively high, generally achieving 70% to 80%, and the application is also wide. Because the oscillation frequency of this control method is not continuous, the switching frequency is not easy to control. The load voltage ripple coefficient is also relatively large, and the adaptability to abnormal loads is poor.
(6) PWM Control Mode Switching Power Supply
PWM LED driver is mainly composed of four parts, input rectification filtering part, output rectification filtering part, PWM voltage stabilization control part, switching energy conversion part.

Figure 3. 1W High Power LED Driver with PWM
The basic working principle of the PWM switching regulator is that when the input voltage, internal parameters, and external load change, the control circuit performs closed-loop feedback through the difference between the controlled signal and the reference signal to adjust the pulse width of the main circuit switching device. This makes the output voltage or current of the switching power supply stable (that is, the corresponding regulated power supply or constant current power supply).
The power supply efficiency is extremely high, generally achieving 80% to 90%, and the output voltage and current are stable. Generally, this kind of circuit has perfect protection measures and is a high-reliability power supply.
3. According to the Installation Location
According to the installation location, the driving power can be divided into the external power supply and the built-in power supply.
(1) External power supply
As the name implies, the external power supply is to the power supply installed outside. Generally, for the circuits with relatively high voltage, which is dangerous to human safety, an external power supply is required. The difference between it and the built-in power supply is that the power supply has a shell, and street lights are common ones.
(2) Built-in power supply
It is to install the power supply in the lamp. Generally, the voltage is relatively low, 12v to 24v, and there is no safety hazard to people. This common one is the bulb light.
V Application
Let's see from the main application market of high-power LEDs-landscape lights, to analyze the high-power LED market.

Figure 4. Landscape Lighting
In China, as the largest application market of LED lighting, the landscape lighting market accounts for about 43%. Its new round of rapid growth will surely drive the rapid development of the overall LED lighting industry.
The landscape lighting of some large and medium-sized cities in such as Shanghai, Xiamen, Beijing, Dalian, Nanchang, etc. has already achieved a considerable scale, and a considerable part of the LED lighting demonstration projects have been completed. The successful completion of these demonstration projects in large and medium cities and the successful use in the Olympic venues indicates that the technology of LED lighting in landscape lighting has gradually matured.
Whether at home or abroad, the city's landscape is the landmark building product of a city. And neon lights, as landscape lighting, are gradually being replaced by LED landscape lights all over the world due to energy, energy saving, environmental protection, and other issues.
There are about 700 thousand cities around the world and assume a city has 5,000 lamps and a lamp is about 1,000 yuan, the huge economic benefits produced by these alone are unpredictable.
The driver is the core component of LED lighting. With the maturity of LED chip technology, the quality of the LED light source has been very reliable. In many cases, the failure of LED lamps comes from the driver. High-power LED driving power is an emerging industry and has not yet formed a concentrated industry cluster, so the regionality is not obvious. Moreover, there are not many companies entering the industry, so the competition is relatively low.
VI Disadvantages
1. The technical personnel of the company that produces LED lighting and related products does not have enough understanding of the switching power supply. The power supply can work normally, but some key evaluations and electromagnetic compatibility are not considered insufficiently, producing certain hidden dangers;
2. Most of the LED power supply manufacturers are transforming from ordinary switching power supplies to LED power supplies, and they have insufficient knowledge of the characteristics and use of LEDs;
3. There are almost no standards for LEDs, most of them refer to the standards of switching power supplies and electronic rectifiers;
4. Most LED power supplies are not unified, so the number of them is relatively small. Since the purchase amount is small, the price is high, and the component suppliers are not very cooperative;
5. In terms of the stability of the LED power supply, wide voltage input, high and low-temperature operation, over-temperature, over-voltage protection, and other issues have not been solved.
Recommended Articles:
Introduction to Voltage Stabilizer
What is a Digital Integrated Circuit and How Do We Use It?
Introduction to Photonic Integrated Circuits and PIC Technology
1.What does a LED driver do?
An LED driver is a self contained power supply which regulates the power required for an LED or array of LEDs. The light emitting diodes are low energy, lighting devices with a long lifespan and low energy consumption, hence the requirement for specialized power supplies.
2.Do I need a driver for LED lights?
Most LEDs require a driver, a few are designed to run on AC current. Most household LEDs that are direct replacements for incandescent, halogen, and CFL bulbs with an E26/E27 or GU10/GU24 base have an internal driver. It's the strip lights where people trip up.
3.What is an LED driver and power supply?
An electrical circuit that regulates the incoming power to provide a constant-voltage output has typically been referred to as a power supply, whereas an LED driver in the strict sense refers to an electrical circuit that provides a constant current output.
4.How do I choose an LED driver for my LED?
Use an LED driver with at least the same value as your LED(s). The driver must have a higher output power than your LEDs require for extra safety. If the output is equivalent to the LED power requirements, it is running at full power. Running at full power may cause the driver to have a shorter life span.
5.Does LED driver get hot?
Heat is the enemy of electronics and this goes for LED drivers too. This doesn't mean that LED drivers cannot operate in hot environments, they can. But there are some simple precautions you can take to avoid failures due to over temperature. It shows a working temperature range of -40 to +70 degrees Celsius.
Discovering New and Advanced Methodology for Determining the Dynamic Characterization of Wide Bandgap DevicesSaumitra Jagdale15 March 20242276For a long era, silicon has stood out as the primary material for fabricating electronic devices due to its affordability, moderate efficiency, and performance capabilities. Despite its widespread use, silicon faces several limitations that render it unsuitable for applications involving high power and elevated temperatures. As technological advancements continue and the industry demands enhanced efficiency from devices, these limitations become increasingly vivid. In the quest for electronic devices that are more potent, efficient, and compact, wide bandgap materials are emerging as a dominant player. Their superiority over silicon in crucial aspects such as efficiency, higher junction temperatures, power density, thinner drift regions, and faster switching speeds positions them as the preferred materials for the future of power electronics.
Read More
A Comprehensive Guide to FPGA Development BoardsUTMEL11 September 20254127This comprehensive guide will take you on a journey through the fascinating world of FPGA development boards. We’ll explore what they are, how they differ from microcontrollers, and most importantly, how to choose the perfect board for your needs. Whether you’re a seasoned engineer or a curious hobbyist, prepare to unlock new possibilities in hardware design and accelerate your projects. We’ll cover everything from budget-friendly options to specialized boards for image processing, delve into popular learning paths, and even provide insights into essential software like Vivado. By the end of this article, you’ll have a clear roadmap to navigate the FPGA landscape and make informed decisions for your next groundbreaking endeavor.
Read More
Applications of FPGAs in Artificial Intelligence: A Comprehensive GuideUTMEL29 August 20251461This comprehensive guide explores FPGAs as powerful AI accelerators that offer distinct advantages over traditional GPUs and CPUs. FPGAs provide reconfigurable hardware that can be customized for specific AI workloads, delivering superior energy efficiency, ultra-low latency, and deterministic performance—particularly valuable for edge AI applications. While GPUs excel at parallel processing for training, FPGAs shine in inference tasks through their adaptability and power optimization. The document covers practical implementation challenges, including development complexity and resource constraints, while highlighting solutions like High-Level Synthesis tools and vendor-specific AI development suites from Intel and AMD/Xilinx. Real-world applications span telecommunications, healthcare, autonomous vehicles, and financial services, demonstrating FPGAs' versatility in mission-critical systems requiring real-time processing and minimal power consumption.
Read More
Xilinx FPGAs: From Getting Started to Advanced Application DevelopmentUTMEL09 September 20251833This guide is your comprehensive roadmap to understanding and mastering the world of Xilinx FPGA technology. From selecting your first board to deploying advanced AI applications, we'll cover everything you need to know to unlock the potential of these remarkable devices. The global FPGA market is on a significant growth trajectory, expected to expand from USD 8.37 billion in 2025 to USD 17.53 billion by 2035. This surge is fueled by the relentless demand for high-performance, adaptable computing in everything from 5G networks and data centers to autonomous vehicles and the Internet of Things (IoT). This guide will walk you through the key concepts, tools, and products in the Xilinx ecosystem, ensuring you're well-equipped to be a part of this technological revolution.
Read More
The Ultimate Guide to Microchip MCUs: From Selection to Real-World ApplicationsUTMEL13 September 2025817Are you an aspiring electronics enthusiast, a seasoned engineer, or a hobbyist looking to bring your next project to life? If so, you've likely encountered the term Microchip MCU. But what exactly is a Microchip MCU, and how do you choose the right one from their vast portfolio? This comprehensive guide will walk you through everything you need to know about Microchip's powerful microcontrollers, from selection and programming to real-world applications.
Read More
Subscribe to Utmel !
89HT0832PZCHLGRenesas Electronics America Inc.
FOD4216VON Semiconductor
TLE82642EXUMA1Infineon Technologies
FODM3023-NF098ON Semiconductor
AD9941BSTZRLAnalog Devices Inc.
AT88SC3216C-MJMicrochip Technology
SC85410EVTAJD557NXP Semiconductors
AD9960BSTZAnalog Devices Inc.
HCS361/SNMicrochip Technology
AT88SC118-SH-CM-TMicrochip Technology